Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Opening Control Panel

You use Control Panel to get easy access to some of the most used functions on servers in the EcoStruxure BMS.

Mostrar más
action_close

The Control Panel gives you easy access to some of the common functions in the EcoStruxure Building Operation software.

Each EcoStruxure BMS server has a control panel. Para obtener más información, consulte Opening Control Panel .

You access control panel of each of the servers in your EcoStruxure BMS by choosing the server you want to work with in the System Tree Pane, and then clicking on the Control Panel tab. The toolbar icon Control Panel and the item Control Panel in the Tools menu display the control panel for the server you are logged on to.

To get back to the Control Panel when you have entered any of the functions, click the Back button

 
action_zoom_plus_stroke
on the navigation toolbar.

 
action_zoom_plus_stroke Control Panel
Figura: Control Panel

Control Panel displays active links to the features that the logged on user account has permissions for.

To open Control Panel
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  • Control Panel
  • Control Panel Tab