earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WorkStation
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018/10/29

打开对象特定事件视图

您可以浏览与特定对象或特定分支相关的所有事件。

注释:

特定于对象的标准过滤器只能精简事件视图中显示的内容。

显示更多
action_close

You can style certain events to bring out those that are of more interest than other events listed in the Events pane and Event Views. To style a specific event, you first have to create a condition that is associated with the events you want to style. An event can be styled with a unique background color, font, and font color.

For example, you can style all events where an alarm is acknowledged. To separate this event from others you configure, change the background color to dark green and the font color to white. All other events have the default style which is a white background and black font color.

If an event fulfills the condition criteria in more than one of the configured event criteria, it is the event style with highest priority in the Events View Style dialog box that is applied to the event.

Events styling does not apply to WebStation and does not affect the events in WebStation.

Event View standard filter and layout

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users of the the EcoStruxure BMS.

有关更多信息,请参阅 Alarm View and Event View Standard Filter and Layout .

打开对象特定事件视图
  1. 系统树 窗格中,选择要浏览其事件的对象。

  2. 操作 菜单,指向 视图 然后点击 事件 此分支中的事件

  • 事件运作方式
  • 事件窗格和事件视图
  • 事件窗格和事件视图工具栏
  • Actions Menu