Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
All system events, as well as information and circumstances, are recorded in the Event log. These event records can be viewed in the Events pane or in an Event View.
事件可以告知您有人登录或注销 EcoStruxure BMS、更改设定值、在文件中写入通告、发送电子邮件通告和创建对象。例如,事件可以告知您谁在何时创建了趋势日志或报警。事件日志还会记录自动化服务器何时在线或离线,以及软件何时升级。事件日志可用于追踪系统中的所有信息。
要限制在 WorkStation 事件窗格中显示的事件数量,可以使用时间间隔过滤器或许多其他过滤器。指示器会告知您显示事件的数量。
您可以创建和使用多个事件视图。每个事件视图和事件窗格都能通过事件过滤器自定义,以仅显示您感兴趣的信息。
您可以浏览系统中某个对象所生成的所有事件。
在 WorkStation 中,您还可以浏览分支的所有事件。分支可以是包含所有内容的文件夹或网络等。
浏览某个分支的事件时,事件是基于分支路径。这意味着对于移动到分支的对象来说,不具有完整的历史事件列表。如果容器已移动或重新命名,历史事件也会丢失。会显示从容器中移除或删除的对象的事件。
在事件视图中,还可以打开详情视图以检查所选择事件的所有属性。
对于时间表事件,会将更改编码:
周一:WS00001
周二:WS00002
周三:WS00003
周四: WS00004
周五:WS00005
周六:WS00006
周日: WS00007
You can style certain events to bring out those that are of more interest than other events listed in the Events pane and Event Views. To style a specific event, you first have to create a condition that is associated with the events you want to style. An event can be styled with a unique background color, font, and font color.
有关更多信息,请参阅 Events Pane and Event View Customization .
Event filter conditions are used to set up the conditions for the events you want to be displayed in the Events pane or an Event View.
有关更多信息,请参阅 Event Filter Conditions .
When you make layout or filter changes to certain panes and views, you can save the changes as a favorite. The purpose of the favorite is to quickly and temporarily change the Standard layout and narrow what is displayed in the pane or view by applying the favorite filter conditions.
有关更多信息,请参阅 收藏夹 .
Archiving is the process of preserving historical data, which is comprised of selected events and extended trend logs. For example, some facilities are required to maintain archives to comply with government regulations. Another example is in secure facilities where they must maintain records of who logged in or who changed setpoints. Archiving is not a backup function because archive data cannot be imported back into the system.
有关更多信息,请参阅 Archiving Overview .