Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Create Out of Range Alarm Wizard – Alarm Trigger Page

Use the Alarm Trigger page to configure the trigger settings of the out of range alarm.

 
action_zoom_plus_stroke Out of range alarm trigger page
Rysunek: Out of range alarm trigger page

Tabela: Out of Range Alarm Trigger Page

Component

Description

Upper limit

​Enter the highest value the monitored variable can increase to before the alarm is triggered.

Lower limit

​Enter the lowest value the monitored variable can decrease to before the alarm is triggered.

Deadband

​Enter the range the monitored variable has to pass within the normal range before the alarm is reset.

Monitored variable

​Enter the path to the variable that is monitored by the alarm.

Disable alarm

Select to disable the alarm, for example, before deployment.

Alarm delay

​Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered.

Reset delay

​Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset.

Shunt variable 1

​Enter the shunt variable that is used to enable or disable the alarm. Więcej informacji zawiera Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Więcej informacji zawiera Shunt Variables .

Operator

Select AND or OR to add logic between the first and the second shunt variable. Więcej informacji zawiera Shunt Variables .

Shunt variable 2

​Enter the second shunt variable that is used to enable or disable the alarm. Więcej informacji zawiera Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Więcej informacji zawiera Shunt Variables .

 
action_zoom_plus_stroke

Set u nit

​Enter the unit of the alarm.

  • Out of Range Alarms
  • Create Alarm Wizard – Presentation Page
  • Create Alarm Wizard – User Action Page
  • Create Alarm Wizard – Attachment Page
  • Out of Range Alarm Properties – Basic Tab
  • Create Object Dialog – Naming the Object Page