earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2.0, 2.1, 3.0, 3.1
2019/1/8

Pane Properties

Use the Pane properties to configure the settings of the pane.

 
action_zoom_plus_stroke Pane properties
图: Pane properties

表格: Pane Properties

Component

Description

Show toolbar

Select Yes to show the toolbars for the pane component.

Default dock position

Select where to place the pane in the workspace.

Default visibility

Select Hidden to hide the pane.

Dipslay name

Type the pane name that is to be displayed. Display name is available only in Workstation.

Initial path

Enter the path to the pane component.

  • Workspace Management
  • General Information Properties – Basic Tab