earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2.0, 2.1, 3.0, 3.1
2019/1/8

Panel Properties

Use the Panel properties to configure the properties of a panel.

 
action_zoom_plus_stroke Panel properties
图: Panel properties

表格: Panel Properties

Component

Description

Work area initial path

Enter the path, for example a graphical link, that points to the panel.

Show toolbars

Select Yes to show the toolbars of the panel.​

 
action_zoom_plus_stroke

Add

Click to add a pane component to the panel. 有关更多信息,请参阅 Create Object Wizard – Naming the Object Page .

 
action_zoom_plus_stroke

Edit

Click to edit a pane component. 有关更多信息,请参阅 Pane Properties .

 
action_zoom_plus_stroke

Remove

Click to remove a panel component.

  • Panel Components
  • Create Object Wizard – Naming the Object Page
  • General Information Properties – Basic Tab