earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2023
12/16/2022

Progress View

The Progress view displays information about time-consuming operations between WorkStation and the EcoStruxure BMS server.

 
action_zoom_plus_stroke The Progress view
Figure: The Progress view

Table: Progress View

Component

Description

Operation

Displays the name of the operation that is being performed.

Name

Displays the name of the object that the operation is performed on.  

Progress

​Displays the progress of the operation so you can determine when the operation is complete.

Status

​Displays the status of the operation.

 
action_zoom_plus_stroke

Click to get details for the operation.

Close

Click to close the Progress view dialog box.

  • Operation Details Dialog Box
  • Error Details – Progress View