WebStation has a many functions that help you work efficiently. You can search for and organize objects, and you can get help using the online help.
You log on to WorkStation or WebStation to securely access the EcoStruxure BMS features.
For more information, see WebStation or WorkStation Login .
You can change regional settings and use different themes to adapt WebStation to your region and your screen.
For more information, see Regional Settings and Theme Settings .
The workspace in WorkStation and WebStation is the area where you perform all tasks at your site, such as acknowledging alarms and viewing trend logs.
For more information, see Workspaces .
WebStation has features to help you in your daily work. For example, you can search for, sort, and filter objects.
For more information, see Search, Sort, and Filter .
You can change and force values using a graphic or the Properties pane. Using the Watch pane, you can dynamically monitor a value.
For more information, see Modify Values .
The EcoStruxure BMS Help provides you with information on how to handle and understand the system.
For more information, see Help in WebStation .
For security reasons, the default configuration for WebStation is, for example, not to allow external content to be embedded.
For more information, see Security Configuration in WebStation .
WebStation supports disabling of unnecessary animations. The disabling can only be done in the operation system. To disable unnecessary animations, refer to your operation system. The disabling of unnecessary animations does not affect animated graphics, such as TGML graphics in WebStation.