earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Conceito

Conceito


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Funcionalidade básica
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Quick Filter

You use Quick filter to filter out the objects by their names from the list. You can either type the name in the Quick filter box or drag an item from a column in the Alarms pane, the Events pane, an Alarm view, or an Event view and drop it in the Quick filter box.

For example, if you want to find all objects that are named “temperature”, just type “temp” in the Quick filter box and only objects named temperature are displayed in the list. 

 
action_zoom_plus_stroke Filtering on characters in all visible columns
Imagem: Filtering on characters in all visible columns

The Quick filter filters on everything that is visible in the columns of the view. For example, if you filter on “20” you do not get any hits. But if you add the column Value, you get hits on the temperature, which is 20, and the setpoint which is 20.

The Quick filter for the Event View filters on records that have already been retrieved from the server.

 
action_zoom_plus_stroke Quick filter filters on all visible columns in the view
Imagem: Quick filter filters on all visible columns in the view

​Quick filter is used in the following components in WorkStation:

  • ​List View

  • Alarms pane

  • Alarm Views

  • Events pane

  • Event Views

  • Alarm or Event details views

  • Watch pane

  • Watch Views

  • Add/Remove columns dialog box

  • Create object wizard

 
action_zoom_plus_stroke The Quick filter is used in many components, such as the List View (upper left), the Watch pane (bottom left), and the Add/Remove dialog box (upper right).
Imagem: The Quick filter is used in many components, such as the List View (upper left), the Watch pane (bottom left), and the Add/Remove dialog box (upper right).
  • Funções básicas
  • Alarms Pane and Alarm View
  • Alarm and Event Detail View
  • Painel de monitorização ou vista de monitorização
  • Add/Remove Columns Dialog Box (List View)