earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
7/19/2021

Archive Log Contents

You use a structured database editor to view archive information in rows and columns, which may contain text strings, paths, identities, or enumeration values.

 
action_zoom_plus_stroke Archive data displayed in a spreadsheet editor
Figure: Archive data displayed in a spreadsheet editor
Note:

The time stamps for each record in the archive file reflect the UTC rather than local machine time.

Columns and Descriptions

The following table provides an overview of an archive file. The number and type of columns that display varies with the log that is viewed. For example, trend logs have a different set of column headers than event logs due to the data content.

Table: Archive Files – Column and Descriptions

Column

Description

AcknowledgeTime

Displays the time and date when the alarm was acknowledged.

AlarmState

Displays the present alarm state.

AlarmText

Displays the alarm message that was added to the alarm.

AssignedState

Displays the assigned state the alarm had.

AssignedToDomain

Displays the domain to which the user or group was assigned.

AssignedToName

Displays the name of the user or group to which an alarm was assigned.

AssignedToUniqueUserId

Displays the unique ID of the user or group to which an alarm was assigned.

BACnetEventType

Displays the BACnet event that occurred within a BACnet network.

BasicEvaluationState

Displays the basic evaluation state of an alarm.

Category

Displays the name of a category.

Command

Displays the executed command.

Comment

Displays the comment that was added to an alarm.

ControlDescr

Displays the descriptive information about the I/NET operator.

ControlSource

Displays the initials of the controlling I/NET operator.

Count

Displays the number of times the alarm has toggled between the alarm and reset state.

CWSId

Displays the ID of the EcoStruxure Web Service (EWS) object.

CWSSourceId

Displays the ID of the EWS source object.

CWSSourceName

Displays the name and path of the EWS source object.

Description

Displays a brief summary of the major features or characteristics.

DeviceName

Displays the name of an I/NET device that generated the event.

DisabledCause

Displays the reason why the alarm was disabled, such as a shunt variable.

DomainName

Displays the domain to which a user belongs.

EndTime

Displays the time when the old meter was replaced.

EndValue

Displays the value the old meter had when it was replaced.

EvaluationState

Displays the present evaluation state of the alarm, such as Upper limit alarm.

Event

Displays an event that occurred within the network.

EventGUID

Displays the unique identity of the event.

FirstName

Displays the first name of the individual whose key/card was used at the I/NET door point.

ForcedValue

Displays the forced value events.

GroupName

Displays the name of the cause note or action note group the user edited.

Hidden

Displays the visible status of an object, such as False.

InetAddr

Displays the system address of the point, or station address of the host or controller that generated the event.

IndivNdx

Displays the number of the individual whose key/card was used at the I/NET door point.

InetEventTypeId

Displays the IDs of the I/NET event types generated by the system.

ItemName

Displays the name of the check list, cause note, or action note group the user edited.

LastName

Displays the last name of the individual whose key/card was used at the I/NET door point.

LinkName

Displays the name assigned to the link of the device from which the event originated.

LogType

Displays the type of the trend log that has been edited.

MaxValue

Displays the last value of the new meter before roll-over.

MessageText

Displays the text of an I/NET action or dispatch message. (Optional)

MeterConstant

Displays the constant of the meter in a meter trend log.

MinValue

Displays the first value of the new meter after roll-over.

MonitoredValue

Displays the path of the monitored variable.

MonitoredValueType

Displays the type of monitored value that triggers an alarm, such as Forced.

MonitoredVariable

Displays the path of the monitored variable.

Note

Displays the text entered into the Note 1 property.

OriginalSeqNo

Displays the RefSeqNo collected from a trend log. This number is only written on an extended trend log containing records that were changed on the connected trend log.

OriginatedGUID

Displays the unique identity of the source.

PreviousAlarmState

Displays the previous alarm state.

Priority

Displays the current priority of the alarm.

RefSeqNo

Displays the unique sequence number of a record that has been edited.

SEQNO

Displays the sequence number of the record.

ServerOffline

Displays the online/offline status of an EcoStruxure BMS server.

Source

Displays the name and path of the source object.

SourceServer

Displays the name and path of the source object.

StationName

Displays the name assigned to the controller from which the event originated.

StartTime

Displays the time when the new meter was installed.

StartValue

Displays the value of the new meter when it was installed.

Status

Displays the status of the trend log.

SystemAlarmId

Displays the alarm ID generated by the system.

SystemEventId

Displays the event ID generated by the system.

TenantNdx

Displays the tenant number of the individual whose key/card was used at the I/NET door point.

TextField

Displays the information entered into the Text property.

TimeStamp

Displays the date and time when the record was generated.

TriggeredTimestamp

Displays the time and date an alarm went from normal state to alarm state.

TYPE

​Displays the object type that defines the properties of the object.

UniqueAlarmId

Displays the unique alarm ID of an alarm.

UniqueUserId

Displays the unique identity number of a user.

Unit

Displays the selected unit of a value, such as °F (Fahrenheit).

User

Displays the user who generated the event.

UserName

Displays the name of the user who generated the event.

Value

Displays the value of a record.

ValueAfter

Displays the value of an object after it was changed.

ValueBefore

Displays the value of an object before it was changed.

Zone

Displays the I/NET security zone number associated with a security event.

Event and Alarm Enumerations

An enumeration is a range of values representing a specific command or event.

For more information, see Event and Alarm Enumerations .

Trend Log Enumerations

An enumeration is a range of values representing a specific command or event. Trend log properties use two enumeration values: Events and Status.

For more information, see Trend Log Enumerations .

  • Archive Folders, Files, and Names
  • Trend Log Enumerations
  • Event and Alarm Enumerations