earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: ​License Administrator, ​License Server
功能: 基本功能
产品版本: 1.8, 1.9
2015/6/25

Reinstalling the License Administrator and the License Server

​You reinstall the License Administrator and the License Server to replace your current installation with a fresh copy.​

显示更多
action_close

This is an additional solution instead of first manually uninstalling the current product and then installing a new copy.

通知

数据丢失

Back up the Enterprise Server before reinstalling the product. ​All​ user settings, database information, and system files related to this product are erased and replaced. 有关更多信息,请参阅 Backing Up SmartStruxure Servers Manually .

不遵照这些说明可导致数据丢失。

To replace your current version, you start with the installation package of the product you want to reinstall. If the installation package recognizes an earlier installation of the Building Operation product within the same major and minor version number but lower maintenance number, the installation wizard asks if you want to uninstall the current version before installing this package. 

注释:

Before reinstalling a License Server or Enterprise Server, you must stop related Windows services.

To reinstall the License Administrator and License Server
  1. On the License Server, open the Service management console.

    注释:

    In Windows, open the Run dialog box and enter services.msc

  2. Right-click Building Operation x.x License Server .

     
    action_zoom_plus_stroke
  3. Select Stop .

  4. Double-click on the License Administrator installation file to start the installation wizard.

  5. Click Yes , to confirm that you want to run the License Administrator installation package.

     
    action_zoom_plus_stroke
  6. Click Next .

     
    action_zoom_plus_stroke
  7. Make sure that you agree with the End User License Agreement (EULA) and then click I Agree .

     
    action_zoom_plus_stroke
  8. Click Next .

     
    action_zoom_plus_stroke
  9. Select the components you want to reinstall and then click Next .

     
    action_zoom_plus_stroke
  10. Select Uninstall current version before reinstalling to reinstall the current License Administrator installation.

     
    action_zoom_plus_stroke
  11. Click Next .

  12. In the License Server Address box, type @ and then type the address to the license server.

    注释:
    • If the License Server uses a port other than the default port range 27000-27009, type the port number in front of @. For example, 567@localhost.

    • Use a semicolon to separate addresses to different License Servers.

     
    action_zoom_plus_stroke
  13. Click Install .

  14. Click Next .

     
    action_zoom_plus_stroke
  15. Click Finish .

     
    action_zoom_plus_stroke
  • Stopping the License Server
  • Installation Wizard – Installation Type Page
  • Installation Wizard – Choose Components Page
  • Reinstallation
  • Installation Wizard – License Server Configuration Page