earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 1.8, 1.9
2016/10/13

Backing Up SmartStruxure Servers Manually

You back up multiple SmartStruxure servers manually to copy and store data that is frequently updated.

显示更多
action_close

Manual Backup is a non-automated process of copying and storing data on a selected SmartStruxure server. You can use this option to create backups on an as-needed basis. You can also manually restore the data at any time.

You log on to one of the following SmartStruxure servers to initiate a manual backup:

Backup Set Naming

For manual backups, the system initially names the backup set by combining the SmartStruxure server name with the localized date and time of the machine running WorkStation. For scheduled backups, however, the system combines the SmartStruxure server name with the UTC time in the backup set name rather than the local time.

提示:

The system also retains the UTC time of manually generated backups. To view the UTC time rather than the localized time for a manual backup set, select the Backup date property from the column selector of the Backup Sets List view. 有关更多信息,请参阅 Columns .

If you log on to the Enterprise Server in WorkStation to create a backup of the SmartStruxure server device, the system automatically checks for identical backup set names. If a name is found in the AS Archives folder, the system warns of a potential duplication by highlighting the Backup set name prefix box or the Backup set name suffix box in solid red. If you do not change the prefix or suffix, the system displays a red box around the backup set in the Backup set name column to indicate that there is an existing name. If you still do not change the name, the system automatically appends an extended time stamp to prevent the accidental overwriting. 有关更多信息,请参阅 Duplicate Backup Set Names in Multi-server Systems .

Local Backup and Restore of SmartStruxure Servers

In WorkStation, you can log on to a SmartStruxure server directly to perform manual backup and restore tasks.

有关更多信息,请参阅 Local Backup and Restore of SmartStruxure Servers .

Remote Backup and Restore of SmartStruxure Server Devices

When you log on to an Enterprise Server, you can perform remote backups of any SmartStruxure server devices in the system. Whenever a backup occurs on the SmartStruxure server device, the system overwrites the locally stored file on the SmartStruxure server device with the new backup file. The Enterprise Server then retrieves and stores this backup file in a separate directory on the computer that runs the Enterprise Server.

有关更多信息,请参阅 Remote Backup and Restore of SmartStruxure Server Devices .

To back up SmartStruxure servers manually
  1. In WorkStation, in the System Tree pane, select the SmartStruxure server.

  2. On the Actions menu, click Backup .

  3. In the Backup set name prefix box, type some text at the beginning of the file name that helps identify the backup set.

     
    action_zoom_plus_stroke
  4. In the Backup set name suffix box, type some text at the end of the file name that helps identify the backup set.

  5. In the Include column, select the SmartStruxure servers that you want to include in the backup, or click the Select All button

     
    action_zoom_plus_stroke
    to include all the listed SmartStruxure servers in the backup.

  6. In the Backup content column, select the type of data you want to back up for each SmartStruxure server:

    • Select Configuration only to back up the configuration database and custom object type data.

    • Select All data to back up the configuration, historical data, and custom object type data.

  7. In the Backup set description column, type a brief description up to 255 characters to help identify the content of each backup.

     
    action_zoom_plus_stroke
  8. Click the Synchronize Description button

     
    action_zoom_plus_stroke
    to add the same backup set description entered for one SmartStruxure server to all the other backup sets.

  9. Click the Synchronize Content button

     
    action_zoom_plus_stroke
    to add the same content type chosen for one SmartStruxure server to all the other backup sets.

  10. Click the Synchronize All button

     
    action_zoom_plus_stroke
    to add both the backup set description and the content type chosen for one SmartStruxure server to all the other backup sets.

  11. Click Backup .

  12. Verify that the backups succeeded and click Close .

     
    action_zoom_plus_stroke
  • Manual Backups
  • Mass Backup
  • Synchronizing SmartStruxure Server Backups on a Network
  • Checking the Backup Status of a SmartStruxure Server
  • Backup Options Dialog Box