When you log on to an Enterprise Server, you can perform remote backups of any SmartStruxure server devices in the system. Whenever a backup occurs on the SmartStruxure server device, the system overwrites the locally stored file on the SmartStruxure server device with the new backup file. The Enterprise Server then retrieves and stores this backup file in a separate directory on the computer that runs the Enterprise Server.
When you want to restore a SmartStruxure server device, the system displays only the valid SmartStruxure server device backup files that are stored on the Enterprise Server.
In the event that the backup file on the SmartStruxure server device is damaged or lost, or not the one you want to use, you can select a valid backup file to restore the SmartStruxure server device. The restore operation overwrites the locally stored SmartStruxure server device backup file located on the SmartStruxure server device with the selected backup file. 有关更多信息,请参阅 Restoring a SmartStruxure Server Device from the Enterprise Server .