earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: ​License Administrator, ​License Server
功能: 基本功能
产品版本: 2024, 7.0
2024/12/2

​Repairing the License Administrator and the License Server

​​You repair the License Administrator and the License Server installation if any problems are caused by the current installation.

显示更多
action_close

If something unexpected happens to an EcoStruxure Building Operation product, for example, the EcoStruxure Building Operation product does not start or software files are missing, you can try to solve the problem by repairing the installation.

To repair an installation you must have access to the installation package that was used to install the product. When starting the installation the wizard asks if you want to reinstall or repair the current installation. When repairing an EcoStruxure Building Operation product, the current product related database, files created by the user, and user settings are kept intact. System files are replaced with the files from the installation package.

注释:

Before repairing a License Server or Enterprise Server, you must stop related Windows services.

重要:
  • To repair an installation, you must have access to the installation package that was used to install the product.

To repair the License Administrator and License Server
  1. On the License Server, open the Service management console.

    注释:

    In Windows, open the Run dialog box and enter services.msc

  2. In the Services console, right-click Building Operation x.x License Server .

  3. Select Stop .

  4. Double-click on the License Administrator installation file to start the installation wizard.

  5. Click Yes to confirm that you want to run the License Administrator installation package.

  6. Click Next .

  7. Make sure that you agree with the End User License Agreement (EULA) and then click I Agree .

  8. In the Program Files page, click Next .

  9. In the Choose Components page, select the components you want to repair and then click Next .

  10. In the Installation Type page, select Repair current version to repair the current License Administrator installation.

  11. Click Next .

  12. In the License Server page, in the License Server Address box, type @ and then type the address to the license server.

    注释:
    • If the License Server uses a port other than the default port range 27000-27009, type the port number in front of @. For example, 567@localhost.

    • Use a semicolon to separate addresses to different License Servers.

  13. Click Install .

  14. In the Installation Complete page, click Next .

    注释:

    Click Show details to follow the progress of the installation.

  15. Click Finish .

  • Stopping the License Server
  • Installation Reparation
  • Products
  • Installation Wizard – Choose Components Page
  • Installation Wizard – Installation Type Page
  • Installation Wizard – License Server Configuration Page