earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos WebReports
Funcionalidades: Informes
Versión del producto: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
16/12/2021

Report Manager Properties – Basic Tab

Use the Basic tab to configure and set up WebReports in WorkStation.

 
action_zoom_plus_stroke Basic tab
Figura: Basic tab

Tabla: Basic Tab

Property

Description

Web site URL

Type the URL of the WebReports Web site. The URL includes the IP address of the Reports Server that is specified during the installation of WebReports.

Type the complete URL, for example, http://10.159.17.246/SchneiderElectric/WebReports/Login.aspx

Web service URL

Type the URL of the WebReports Web service that requests and receives report names, and authenticates user logon information. The URL includes the IP address of the Reports Server that is specified during the installation of WebReports.

Type the complete URL, for example, http://10.159.17.246/SchneiderElectric/WebReportsService

Report source

Verify that the default, WebReports , is selected. Do not change the default Report source .

Default Report Folder Name

Displays the name of the folder in the System Tree pane that is populated with factory supplied reports when WebReports is installed. You open the folder to select and view the factory supplied reports. You can also create and organize your own custom reports in the folder. Do not rename the folder.

  • WebReports Configuration
  • General Information Properties – Basic Tab