earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
5
如何

如何


产品: AS-L, AS-B, AS-P
功能: 硬件
产品版本: 1.8, 1.9
2017/10/12

Resetting a SmartStruxure Server Device to DFU Mode

If the SmartStruxure server device firmware is damaged, the SmartStruxure server device can be put in DFU (Device Firmware Upgrade) mode to be able to communicate on the USB device port.

After the reset operation and the initial boot process, the upgrade process can be started, using the USB device port. It is also possible to retrieve debug information from the device.

显示更多
action_close

There are four different types of reset for the SmartStruxure server devices: warm start, cold start, reset, and reset to DFU mode. Depending on the type of reset, the SmartStruxure server device can be reset using the reset button or a command from WorkStation.

 
action_zoom_plus_stroke Location of reset button and USB device port on different SmartStruxure server device models
图: Location of reset button and USB device port on different SmartStruxure server device models

表格: SmartStruxure Server Device Reset Functions

Type

Triggered by

Description

Variable values

Configuration, Historic database

IP settings

Warm start

Command from WorkStation

Stops the SmartStruxure server device application and then restarts the application.

Affected according to the configured retain levels for the variables

Retained

Retained

Cold start

Command from WorkStation

Stops the SmartStruxure server device application and then restarts the application.

Affected according to the configured retain levels for the variables

Retained

Retained

Reset

Short push on Reset button

Power return

Stops the SmartStruxure server device application and the operating system and then restarts the operating system and the application.

Affected according to the configured retain levels for the variables

Retained

Retained

Reset to DFU mode

3 pushes on Reset button within 2 seconds

Puts the SmartStruxure server device into DFU mode, which enables Device Administrator to communicate with the server.

Not applicable

Not retained

Not retained

Parameters and variables that are used to define the system or contain important data in the SmartStruxure server device can be retained in a permanent memory. These parameters and variables are automatically saved in the event of power failure, or request for restart and are reloaded after startup.

You can define what kind of events that retention for the parameters and variables should apply.

Retain Levels for Variables

Variables have a configurable retain level, which controls if the value of the variable is retained after a restart of the SmartStruxure server device. There are three retain levels:

  • No

  • Warm start

  • Cold start

The following table lists what is retained after a warm start, cold start, or reset based on the configured retain level.

表格: Retained Variable Values Depending on Reset Type and Retain Level

Reset type

Retain level: No

Retain level: Warm start

Retain level: Cold start

Warm start

Default value a

Variable retains last value configured by a user. Values set by an application are retained. 

Variable retains last value configured by a user. Values set by an application are retained. 

Cold start

Default value a

Variable retains last value configured by a user. Values set by an application are lost.

Variable retains last value configured by a user. Values set by an application are retained. 

Reset

Default value a

Variable retains last value configured by a user. Values set by an application are retained. 

Variable retains last value configured by a user. Values set by an application are retained. 

  1. Default value is the value the variable gets when it is created.

有关更多信息,请参阅 Retain Level .

Configuration and Historic Database

A number of parameters describe the current configuration. The historic database contains information collected from different sources. Parameters and historic database are retained at both Warm and Cold start.

DFU Mode

The Device Firmware Upgrade mode can be used if the SmartStruxure server device does not communicate in its normal operating mode. In the DFU mode, with a PC connected to the USB device port on the SmartStruxure server device, the Device Administrator can be used to update the firmware. 有关更多信息,请参阅 Resetting a SmartStruxure Server Device to DFU Mode .

To reset a SmartStruxure server device to DFU mode
  1. Start the Device Administrator. 有关更多信息,请参阅 Connecting to a SmartStruxure Server Device Using the USB Device Port .

  2. On the SmartStruxure server device, press the Reset button 3 times within 2 seconds.

     
    action_zoom_plus_stroke
  3. Use a USB cable to connect the USB device port on the SmartStruxure server device with a USB port on the PC.

  4. Ensure that the SmartStruxure server device is displayed in the list and DFU mode is displayed in the Device status column.

The SmartStruxure server device is now ready for the upgrade procedure. 有关更多信息,请参阅 Uploading and Upgrading a SmartStruxure Server Device .

Alternatively, the Device Administrator can now be used to fetch saved debug data. 有关更多信息,请参阅 Getting SmartStruxure Server Device Debug Information .

  • Reset Functions
  • Connecting to a SmartStruxure Server Device Using the USB Device Port
  • Uploading and Upgrading a SmartStruxure Server Device
  • Downloading an Upgraded Database to a SmartStruxure Server Device
  • Getting SmartStruxure Server Device Debug Information