earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool, WebStation
Funcionalidades: Programaciones
Versión del producto: 2023
14/03/2024

Tipos de programaciones

You can create three types of schedules: Digital, Multistate, or Analog. You create a digital schedule if the schedule needs to control a device with two output states, such as On or Off. You create a multistate schedule if the schedule needs to control a device that has output states based on multiple states, such as low, medium, or high. You create an analog schedule if the schedule controls a device that gauges the output in real numbers.

Puede crear programaciones usando WorkStation.

Programaciones analógicas

An analog schedule controls a device that gauges the output in real numbers. The real numbers include positive or negative numbers, fractions, and decimal values.

Para obtener más información, consulte Programaciones analógicas .

Programaciones digitales

A digital schedule controls a device that has an on output state and an off output state.

Para obtener más información, consulte Programaciones digitales .

Programaciones multiestado

A multistate schedule controls a device that has output states based on integers or positive whole numbers including zero.

Para obtener más información, consulte Programaciones multiestado .

  • Programaciones analógicas
  • Programaciones digitales
  • Programaciones multiestado