earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
5/18/2018

Editing or Deleting a Weekly Event in a Xenta Schedule in WebStation

You edit a weekly event to change the time range, start and stop time, or weekdays of the weekly event.

Show More
action_close

Xenta Time Schedules and Xenta Central Time Schedules can be edited in WebStation. You can add, edit and delete weekly and exception events. The Xenta Time Schedules and Xenta Central Time Schedules must be created using WorkStation.

For more information, see How Schedules Work .

Xenta Central schedules are used to group Xenta 280/300/401 LonWorks device schedules created in the TSCH block in Menta Editor. When you use a Central schedule, you can change settings on whole Xenta schedule groups from a central place.

For more information, see Xenta Central Schedules .

Important:

You cannot add, edit, or delete schedule events in a Xenta Schedule when a Xenta Central schedule has been assigned to it.

The number of events a Xenta Central schedule can have is determined by the Menta application.

To edit or delete a weekly event in a Xenta schedule in WebStation
  1. In WebStation, in the System Tree pane, select the schedule containing the weekly event you want to edit.

  2. In the Interval type column, edit Interval or On all day .

  3. If you select Interval , edit the start time and the end time.

  4. Edit the weekdays the weekly event is to be in service.

  5. Click Save .

To delete a weekly event, click the trash can.

  • Xenta Schedules in WebStation
  • Adding a Weekly Event to a Xenta Schedule in WebStation