earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 7.0
19/12/2024

Searching for Objects or Properties

You use this procedure to find objects or properties in the database.

Afficher plus
action_close

Use Search in WorkStation to find and view objects in the database.

There are two different ways to search in WorkStation, simple search and search. A search can be done on, for example, conditions or objects types. A search can be saved for further use.

Search is case insensitive, which means that search does not differ between upper case and lower case. A search on "Fan"displays search results spelled both "fan" and "Fan".

Simple Search

Use Simple Search to search for object names.

Use the Search view to search for names of properties. Pour plus d'informations, voir Searching for Objects or Properties .

Pour plus d'informations, voir Simple Search .

Search

You use search to find objects and properties in the EcoStruxure Building Operation database.

Pour plus d'informations, voir Search .

Saved Search

Frequently used searches including the settings can be saved and reused.

A saved search is displayed in the System Tree pane and the List View. To perform the search, open the saved search from the System Tree pane or List View. The search results are displayed in the work area (with collapsed search criteria area).

A saved search can be changed, renamed, and deleted.

Déclaration
  • When you save a search, only the setting for the search is saved. The search result is never saved.  

Relative or Locked Search Path

If you want to reuse your saved search object in similar folder structures, you can enter a relative search path in your saved search object. You can reuse a saved search object by using export and import or copy and paste special.

If you have configured your search object with a relative reference, the search result is performed on a path relative to the location of the saved search object.

If you have configured your search object with a locked reference, the search is performed on the specific folder or container object even if the folder or container object is renamed or moved. By default, search paths are locked.

Table : Locked and Unlocked References

Path reference syntax

Description

~

Locked reference

Searches in the configured folder or container object

../..

Relative reference

Searches in a path relative to where the search object is saved. For example, entering '../../' in the folder path means that the search is performed two levels up from where the search object is saved.

To search for objects or properties
  1. In WorkStation, on the WorkStation Toolbar menu, click the Search button

     
    action_zoom_plus_stroke
    .

  2. Click the General tab.

  3. In the Search view, in the text box, type the name of the object you want to search for.

  4. In the In folder box, enter the folder where you want to start the search.

  5. In Additional search locations , click Add to add additional search locations.

  6. In the Select Object dialog box, select the reference type and folder or container object where you want to search, and then click Select .

  7. Select Search for properties to only search for properties.

  8. Select Include subservers to include EcoStruxure BMS subserver devices in the search.

  9. Select Stop if more than 1000 results to stop the search at 1,000 results.

  10. In the Include types box, enter the object types to include in the search.

  11. In the Select Types dialog box, select the object types you want to include in the search.

  12. Click the Add type button

     
    action_zoom_plus_stroke
    .

  13. Click OK .

  14. In the Conditions box, enter the conditions to include in the search.

  15. In the Select Conditions dialog box, click the Add condition button

     
    action_zoom_plus_stroke
    to add a search condition.

  16. Click OK .

  17. Click the Search button

     
    action_zoom_plus_stroke
    .

Search results are displayed in the Search result area.

  • Search Overview
  • Chercher
  • Search View
  • Select Folder Dialog Box
  • Searching for Forced Values
  • Select Conditions Dialog Box