earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 3.2, 3.3
12/9/2020

Software Permissions

arrow1_rotationPath Permissions arrow1_rotationCommand Permissions arrow1_rotationExtended Software Permissions arrow1_rotationRelative Path Permissions arrow1_rotationType Permissions arrow1_rotationSoftware Permissions Management

Software permissions are used to manage privileges that user account groups and user accounts own to objects in Building Operation software. In the EcoStruxure Building Operation software, you can assign two types of software permissions to user account groups and user accounts: path permissions and command permissions. You can also assign extended permissions to all the instances of folder structure or of a custom type.

Path Permissions

​Path permissions are used to give a user account group or a user account access to the objects defined in the path. The permissions configured on a path apply to all path sub-levels unless you configure new permissions for the path sub-level.

For more information, see Path Permissions .

Command Permissions

Command permissions grant a specific set of permissions to a user account or a user account group to commands in the EcoStruxure Building Operation database. You use command permissions to configure exceptions from path permissions.

For more information, see Command Permissions .

Extended Software Permissions

Extended Permissions are used to manage privileges of a user account group or a user account with respect to the instances of a folder structure or to the instances of custom type.

There are two types of extended software permissions:

Relative Path Permissions

Relative path permissions for a folder structure grant a specific set of permissions to a user account group or to a user account to all the folders accessible in a predefined path and its folder structure. Relative path permissions enable a user accounts group or a user account to reuse a specific path permission.

For more information, see Relative Path Permissions .

Type Permissions

Extended permissions for a type grant a specific set of permissions to a user accounts group or to a user account to all instances of this type. There are two types of type permissions. Custom type permissions grant permissions for types created by the users. In-build type permissions grant permissions for types provided by default with the system.

For more information, see Type Permissions .

Software Permissions Management

Software permissions can be combined between them.

For more information, see Software Permissions Management .

  • User Account Management Overview
  • Path Permissions
  • Command Permissions
  • Extended Software Permissions
  • Relative Path Permissions
  • Type Permissions
  • Software Permissions Management