earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WebStation
Funktionaliteter: Tidsscheman
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
2018-05-18

Editing or Deleting an Exception Event in a Xenta Schedule in WebStation

You edit an exception event to change the time range, start and stop date, start and stop time, or weekdays of an exception event.

Visa mer
action_close

Xenta Time Schedules and Xenta Central Time Schedules can be edited in WebStation. You can add, edit and delete weekly and exception events. The Xenta Time Schedules and Xenta Central Time Schedules must be created using WorkStation.

Mer information finns i How Schedules Work in Building Operation .

Xenta Central schedules are used to group Xenta 280/300/401 LonWorks device schedules created in the TSCH block in Menta Editor. When you use a Central schedule, you can change settings on whole Xenta schedule groups from a central place.

Mer information finns i Xenta Central Schedules .

Obs!

You cannot add, edit, or delete schedule events in a Xenta Schedule when a Xenta Central schedule has been assigned to it.

The number of events a Xenta Central schedule can have is determined by the Menta application.

To edit or delete an exception event in a Xenta schedule in WebStation
  1. In WebStation, in the System Tree pane, select the schedule containing the exception event you want to edit.

  2. In the Interval type column, edit Interval , On all day or Off all day .

  3. Edit the dates.

  4. Click Save .

To delete an exception event, click the trash can.

  • Xenta Schedules in WebStation
  • Adding an Exception Event to a Xenta Schedule in WebStation