earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: WebStation
Funktionaliteter: Tidsscheman
Produktversion: 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
2024-12-17

Xenta Schedules in WebStation

Xenta Time Schedules and Xenta Central Time Schedules can be edited in WebStation. You can add, edit and delete weekly and exception events. The Xenta Time Schedules and Xenta Central Time Schedules must be created using WorkStation.

Mer information finns i How Schedules Work in Building Operation .

Xenta Central schedules are used to group Xenta 280/300/401 LonWorks device schedules created in the TSCH block in Menta Editor. When you use a Central schedule, you can change settings on whole Xenta schedule groups from a central place.

Mer information finns i Xenta Central Schedules .

  • How Schedules Work in Building Operation
  • Adding a Weekly Event to a Xenta Schedule in WebStation
  • Adding an Exception Event to a Xenta Schedule in WebStation
  • Editing or Deleting a Weekly Event in a Xenta Schedule in WebStation
  • Editing or Deleting an Exception Event in a Xenta Schedule in WebStation