earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
4
Concept

Concept


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 3.3
4/27/2023

Backup

arrow1_rotationTypes of Data arrow1_rotationBackup Sets arrow1_rotationScheduled Backups arrow1_rotationManual Backups arrow1_rotationMass Backup arrow1_rotationSystem Backup arrow1_rotationBackup Status

Backup is the process of copying and storing data so that the copy can be used to restore data if a loss occurs. You can also use a backup to revert to an older version. In the EcoStruxure BMS, you can perform backups on an all EcoStruxure BMS servers and their devices. EcoStruxure BMS server backups should take place during non-business hours.

Using WorkStation, you can back up data to the local drive of each installed EcoStruxure BMS server. The EcoStruxure Building Operation software stores the files by date in a predefined directory location on the server to which WorkStation is connected. For more information, see Backup Sets .

Types of Data

The EcoStruxure Building Operation backup function enables you to back up different types of data.

For more information, see Types of Data .

Backup Sets

Backup sets are compressed backup files used for restoring data. The EcoStruxure Building Operation software stores the local backup set for an Enterprise Server or automation servers in the Local folder within the Backup sets folder.

For more information, see Backup Sets .

Scheduled Backups

A scheduled backup is an automated way to back up data on an EcoStruxure BMS server. You can back up EcoStruxure BMS servers individually using each EcoStruxure BMS server’s local backup rule. You can also use backup rules to synchronize the backups of all the EcoStruxure BMS servers on your network.

For more information, see Scheduled Backups .

Manual Backups

Manual Backup is a non-automated process of copying and storing data on a selected EcoStruxure BMS server. You can use this option to create backups on an as-needed basis. You can also manually restore the data at any time.

For more information, see Manual Backups .

Mass Backup

Mass backup is a method of performing a manual, simultaneous backup of all the EcoStruxure BMS servers in the network, which is useful for capturing data at a critical point, such as prior to an upgrade. You can choose which EcoStruxure BMS servers you want to back up along with the type of data for each.

For more information, see Mass Backup .

System Backup

Before upgrading the system, it is strongly recommended that you archive the historical data and back up the EcoStruxure BMS servers to preserve the current data and configurations. If you plan to upgrade WebReports, be sure to back up the Reports database in SQL Server.

For more information, see System Backup .

Backup Status

Backup Status displays the statuses of an EcoStruxure BMS server: Ready, Backing up, or Backup succeeded.

For more information, see Backup Status .

  • Backup and Restore Overview
  • Types of Data
  • Backup Sets
  • Scheduled Backups
  • Manual Backups
  • Mass Backup
  • System Backup
  • Backup Status