earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: Device Administrator, Enterprise Central, Enterprise Server, Function Block Editor, Graphics Editor, License Administrator, License Server, Script Editor, Software Administrator
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Reinstallation

This is an additional solution instead of first manually uninstalling the current product and then installing a new copy.

Uwaga

Loss of data

Back up the Enterprise Server before reinstalling the product. ​All​ user settings, database information, and system files related to this product are erased and replaced. Więcej informacji zawiera Backing Up EcoStruxure BMS Servers Manually .

Failure to follow these instructions can result in loss of data.

To replace your current version, you start with the installation package of the product you want to reinstall. If the installation package recognizes an earlier installation of the EcoStruxure Building Operation product within the same major and minor version number but lower maintenance number, the installation wizard asks if you want to uninstall the current version before installing this package. 

Uwaga

Before reinstalling a License Server or Enterprise Server, you must stop related Windows services.

  • Backing Up EcoStruxure BMS Servers Manually
  • Reinstalling the Device Administrator Installation
  • Reinstalling the Enterprise Server
  • Reinstalling the License Administrator and the License Server
  • Reinstalling WorkStation and Client Tools
  • Installation Overview