You reinstall WorkStation and client tools to replace your current installation with a fresh copy.
For reinstallation, it is assumed that you already have working and available WorkStation, Graphics, Script, and Menta / Function Block licenses. A working license for each product is required to start and log on. If necessary, acquire the needed licenses. Więcej informacji zawiera EcoStruxure Building Operation Software Licensing Installation and Location .
When reinstalling the WorkStation, additional language packages are removed.
Double-click on the WorkStation installation file to start the installation wizard.
If User Account Control (UAC) is enabled on the computer on which you are installing WorkStation, you must run the installer as an administrator. To do this, right-click the WorkStation installation file and then click Run as administrator .
Click Yes to confirm that you want to run Workstation installation pakage.
Click Next .
Make sure that you agree with the End User License Agreement (EULA) and then click I Agree .
In the Installation Folder page, click Next .
Select the components that you want to reinstall and then click Next .
Before selecting the WorkPlace Tech Editor component, be sure the appropriate versions of Microsoft Visio and .NET 3.5 SP1 are installed.
Więcej informacji zawiera EcoStruxure Building Operation Software Requirements .
Select the shortcuts you want to be created and then click Next .
Select Uninstall current version before reinstalling .
Click Next .
In the License Server address box, type @ and then type the address to the license server.
If the License Server uses a port other than the default port range 27000-27009, type the port number in front of @. For example, 567@localhost.
Use a semicolon to separate addresses to different License Servers.
Click Install .
Click Uninstall to remove the current installation.
Click Close .
Click Show details to follow the progress of the installation.
Click Next .
Click Finish .