Use the Alarm Trigger page to configure the trigger settings of the sum alarm.
|
Component |
Description |
|
|
Add condition Select the alarm filter conditions for the alarms you want to include. Więcej informacji zawiera Alarm Filters . You can use wildcards when setting up filter conditions. Więcej informacji zawiera Filter Condition Wildcards . |
|
|
Remove condition Remove the alarm filter conditions for the alarms you want exclude. |
|
Add row Click to add an additional row with the same condition. |
|
Remove row Click to remove a condition row. |
|
Clear all Click to clear the selected conditions. |
|
Alarm State |
Displays the alarm state of the alarm. Więcej informacji zawiera Alarm States . |
|
Matching alarms count |
Displays the number of alarms that currently meet the criteria of the sum alarm. |
|
Disable alarm |
Select to disable the alarm, for example, before deployment. |
|
Alarm delay |
Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered. |
|
Reset delay |
Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset. |
|
Shunt variable 1 |
Enter the shunt variable that is used to enable or disable the alarm. Więcej informacji zawiera Shunt Variables . |
|
Invert |
Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Więcej informacji zawiera Shunt Variables . |
|
Operator |
Select AND or OR to add logic between the first and the second shunt variable. Więcej informacji zawiera Shunt Variables . |
|
Shunt variable 2 |
Enter the second shunt variable that is used to enable or disable the alarm. Więcej informacji zawiera Shunt Variables . |
|
Invert |
Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Więcej informacji zawiera Shunt Variables . |