Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.2, 3.3, 2022
2021-12-17

Synchronized Backups

A synchronized backup is a method of performing a recurring, simultaneous backup of a selected number of EcoStruxure BMS servers. You can use a lead and shadow relationship to automate all the EcoStruxure BMS server backups on your network. Using this method, you configure and manage one lead backup rule on one EcoStruxure BMS server, which other backup rules can reference.

 
action_zoom_plus_stroke Synchronized recurring backup – Lead/Shadow method
Rysunek: Synchronized recurring backup – Lead/Shadow method

The system synchronizes all the shadow rules with the lead backup rule, and all the shadow schedules with the lead schedule. Więcej informacji zawiera Synchronizing EcoStruxure BMS Server Backups on a Network .

  • Backup Rules View