earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.9
14/12/2016

Synchronizing SmartStruxure Server Backups on a Network

You synchronize all SmartStruxure server backups to increase efficiency by centralizing the automated backup management on a single SmartStruxure server, rather than across multiple SmartStruxure servers.

Mostrar más
action_close

A synchronized backup is a method of performing a recurring, simultaneous backup of a selected number of SmartStruxure servers. You can use a lead and shadow relationship to automate all the SmartStruxure server backups on your network. Using this method, you configure and manage one lead backup rule on one SmartStruxure server, which other backup rules can reference.

 
action_zoom_plus_stroke Synchronized recurring backup – Lead/Shadow method
Figura: Synchronized recurring backup – Lead/Shadow method

The system synchronizes all the shadow rules with the lead backup rule, and all the shadow schedules with the lead schedule. Para obtener más información, consulte Synchronizing SmartStruxure Server Backups on a Network .

To synchronize SmartStruxure server backups on a network
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the Enterprise Server.

     
    action_zoom_plus_stroke
  3. Click Backup Rules .

  4. In the Lead rule column, enter a backup rule that you want to use as the lead rule for one or more SmartStruxure servers in the list.

     
    action_zoom_plus_stroke
    Aviso

    When you select a lead rule, the backup rule on a SmartStruxure server becomes a shadow of the lead rule.

  5. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Scheduled Backups
  • Synchronized Backups
  • Removing a Lead Rule from a Backup Rule
  • Editing a Backup Rule
  • Editing a Backup Schedule
  • Backup Rules View