earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-C, AS-B, AS-P, Project Configuration Tool
功能: 本地化
产品版本: 1.9
2024/11/29

Time and Time Zone Configuration in Automation Server

​To adjust the SmartStruxure server device time, time zone, and DST, you have to access the SmartStruxure server device through a WorkStation.

When adjusting the SmartStruxure server device clock, you can either set the time manually or you can refer to a network time server that automatically synchronizes the clock. Manual adjusting is used when you configure or commission a SmartStruxure server device. When the SmartStruxure server device is running on a fully commissioned site, it is important that you use a network time server to avoid drifting time in the SmartStruxure server device.

When adjusting the SmartStruxure server device time through WorkStation, it is the SmartStruxure server device operating system clock you adjust. Building Operation has a transparent layer above the SmartStruxure server device operating system which manages the information about the time zone and DST time offset.

 
action_zoom_plus_stroke  The Automation Server uses the operating system clock to which Building Operation adds the time zone offset and DST
图: The Automation Server uses the operating system clock to which Building Operation adds the time zone offset and DST

Instead of configuring the time of each SmartStruxure server device, you can create a lead and shadow relationship that makes it possible to configure several SmartStruxure server devices through a single Enterprise Server.

  • Lead and Shadow Relationship
  • Synchronize Network Time Settings
  • Synchronize Time Zone Settings
  • Time and Time Zone
  • Regional and Language Overview
  • SmartStruxure Server Device – Date & Time View
  • Manually Changing the SmartStruxure Server Device Time and Date
  • Synchronizing the SmartStruxure Server Device Clock
  • Changing the Time Zone of a SmartStruxure Server