earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos Enterprise Server, Project Configuration Tool
Funcionalidades: Localización
Versión del producto: 1.9
14/12/2016

Time and Time Zone Configuration in Enterprise Server

​The Enterprise Server time and date settings are configured through the operating system settings on which the Enterprise Server is installed. The time zone offset, configured through the Enterprise Server, is added by Building Operation to the UTC time. The Enterprise Server time zone settings are therefore independent of the operating system time zone settings.

 
action_zoom_plus_stroke  The Enterprise Server uses the operating system clock on which the server is installed. Time zone offset and DST are then added by Building Operation to the UTC time.
Figura: The Enterprise Server uses the operating system clock on which the server is installed. Time zone offset and DST are then added by Building Operation to the UTC time.

To adjust your operating system clock, refer to your manufacturer’s manual for the operating system. The Enterprise Server time zone is configured on the Enterprise Server through WorkStation

Aviso
  • The Date and Time synchronization for Automation Server do not affect the Enterprise Server clock. Para obtener más información, consulte Synchronize Network Time Settings .

  • Synchronize Network Time Settings
  • Synchronize Time Zone Settings
  • Time and Time Zone
  • Regional and Language Overview
  • Enterprise Server – Date & Time View
  • Creating a Custom Time Zone of a SmartStruxure Server
  • Configuring Regional Settings