earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: Enterprise Central, Enterprise Server, Project Configuration Tool
功能: 本地化
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
2018/8/21

Time and Time Zone Configuration in Enterprise Server and Enterprise Central

The Enterprise Server and Enterprise Central time and date settings are configured through the operating system settings on which the Enterprise Server and Enterprise Central are installed. The time zone offset, configured through the Enterprise Server or Enterprise Central, is added by the EcoStruxure Building Operation software to the UTC time. The Enterprise Server and Enterprise Central time zone settings are therefore independent of the operating system time zone settings.

 
action_zoom_plus_stroke  The Enterprise Server uses the operating system clock on which the server is installed. Time zone offset and DST are then added by the EcoStruxure Building Operation software to the UTC time.The same is true regarding the Enterprise Central.
图: The Enterprise Server uses the operating system clock on which the server is installed. Time zone offset and DST are then added by the EcoStruxure Building Operation software to the UTC time.The same is true regarding the Enterprise Central.

To adjust your operating system clock, refer to your manufacturer’s manual for the operating system. The Enterprise Server and Enterprise Central time zones are configured through WorkStation.

注释:
  • Synchronize Network Time Settings
  • Synchronize Time Zone Settings
  • Time and Time Zone
  • Regional and Language Overview
  • Date & Time View
  • Creating a Custom Time Zone of an EcoStruxure BMS Server
  • Configuring Regional Settings