The function of a trend log is to log the variable that it is connected to and store the records.
To be able to store larger amount of records, you connect an extended trend log. The records of the trend log and the extended trend log can be presented numerically in a trend log list or graphically in a trend chart. The records can also be processed by a calculation method before they are presented.
A trend log that monitors an enumeration records the enumeration value and not the enumeration definition.
有关更多信息,请参阅 Event and Alarm Enumerations .
有关更多信息,请参阅 Trend Log Enumerations .
You use a trend log to collect data and then store the records. A record contains a log value or an event as well as its time stamp and an optional comment. A trend log can log an analog variable, a digital variable, or an integer variable.
有关更多信息,请参阅 Trend Log Types .
All trend logs store records by using the circular storing principle; you can also connect trends logs to external trend logs with larger storing capacity. For some trend logs you can set up conditions that have to be fulfilled before the trend log starts recording.
有关更多信息,请参阅 Trend Log Functions .
You can define the unit of a trend log when the trend log is created or on a previously created trend log where no unit has been set.
有关更多信息,请参阅 Trend Units .
A trend chart displays the records of a trend log or an extended trend log as a series.
有关更多信息,请参阅 趋势图 .
The trend log list numerically displays the records of a trend log or an extended trend log. The records of the trend log can be processed by a calculation method before they are presented in the trend log list.
有关更多信息,请参阅 Trend Log Lists .
You configure a multi trend log list to display values from multiple trend logs in one list. You compare values in a multi trend log list when you commission or validate an EcoStruxure BMS.
有关更多信息,请参阅 Multi Trend Log Lists .
When moving or copying a trend log or extended trend log to another EcoStruxure BMS server, only the configuration of the trend log is transferred. If you copy the trend log to another EcoStruxure BMS server, all recorded values are preserved in the original trend log while the copy on the other EcoStruxure BMS server does not contain any recorded values. If you move the trend log to another EcoStruxure BMS server, the configuration of the trend log is preserved but the record values are lost.
You use the mass create feature to create multiple identical alarms or trend logs for different objects, instead of creating the alarms or trend logs one by one. From trend logs, you can mass create extended trend logs.
有关更多信息,请参阅 Mass Create .