earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 时间表
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Time Zones

When you create a schedule, the time zone of the EcoStruxure BMS server that contains the schedule determines the execution of the events. If the schedule is copied to an EcoStruxure BMS server in a different time zone, the specified dates and times relate to the new time zone.

For example, a schedule with an event defined to start at 08:00 Eastern Standard Time in a device located in Boston is copied to a device in London. The event would start at 08:00 Greenwich Mean Time.

When working within a schedule, you can display two different time zones. The schedule editor also displays the time differential for the second time zone. For example, if you are working in Eastern Standard Time, the Greenwich Mean Time shows a +5 time differential.

  • Schedules Overview
  • 时间表事件
  • Time and Time Zone