Use the Tools menu to open Control Panel or make a number of user settings.
Command |
Description |
Control Panel |
Click to open the Control Panel where you get access to some of the most used administration functions, such as alarms, domains, user accounts, backup and archiving, and engineering. For more information, see Control Panel Tab . |
Language |
Click to open the Language submenu where you select a different WorkStation language. For more information, see Language Packages . |
Measurement system |
Click to open the Measurement system submenu where you select a different local measurement system. For more information, see Units . |
Database mode |
Click to configure WorkStation to run in database mode so changes are saved to the EcoStruxure BMS server database and not sent to any physical devices. For more information, see Database Mode . |
Options |
Click to open the Options dialog box where you manage some local user settings. For more information, see Options Dialog Box . |