The Top Activities report provides information about the most frequent user and system activities for all EcoStruxure BMS servers in your system. An example of a user activity is creating or changing an object. An example of a system activity is initializing an EcoStruxure BMS server. You can enter a number to filter the top number of activities. You can then determine what activities occur most often on what EcoStruxure BMS servers, and consider ways to improve your system.
The following table shows the input parameters for the report.
Input Parameters |
Description |
Start report date/time |
Specifies the start date and time of the activity period. |
End report date/time |
Specifies the end date and time of the activity period. |
Date range filter |
Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent. For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days. Select Fixed date if you entered a Start report date/time and an End report date/time . |
Hide SystemReportsService activity |
Prevents the SystemReportsService activity from displaying in the report. The SystemReportsService is related to Reporting Agent operations. Use the Hide feature if you do not want the report to display information about the SystemReportsService. |
Report view |
Specifies the format, such as a table, for displaying the report. |
Show top |
Specifies a number used to filter the top most frequently occurring activities. |