The Top System Alarms Per Server report provides information about the most frequently occurring system alarms for a particular EcoStruxure BMS server. The report can be used by System Managers to identify and troubleshoot problems with a specified EcoStruxure BMS server.
The following table shows the input parameters for the report.
Input Parameters |
Description |
Start report date/time |
Specifies the start date and time of the triggered alarms.
|
End report date/time |
Specifies the end date and time of the triggered alarms.
|
Date range filter |
Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent. For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days. Select Fixed date if you entered a Start report date/time and an End report date/time . |
Server |
Specifies the EcoStruxure BMS server that you want to audit. |
Report view |
Specifies the format, such as a table, for displaying the report. |
Show top |
Specifies a number used to filter the top most frequently occurring system alarms. |