earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendências
Versão do produto: 3.2, 3.3, 2022
13-07-2021

Trend Chart Settings Dialog Box – Axes Tab

Use the Axes tab to configure the properties of the chart axes.

 
action_zoom_plus_stroke Axes tab
Imagem: Axes tab

Tabela: Axes Tab

Component

Description

Time mode

​Select the time mode of the x-axis.

Start time

Enter the absolute start time when Time mode is set to Absolute. This time is the leftmost point of the x-axis.

End time

Enter the absolute end time when Time mode is set to Absolute (start time and end time) . This time is the rightmost point of the x-axis.

Time span

Type the relative time span of the x-axis when Time mode is set to Relative (to current time) . The rightmost point of the x-axis is the current time.

Time zone

Select time zone for the trend chart. The time zone is the displayed time perspective of the trend log.

Show grid lines

Select to show horizontal grid lines.

Auto scale left y-axis

Select to activate auto scale. The scale of the left Y-axis adapts itself to the displayed series.

Left y-axis minimum

Type the minimum value of the left y-axis.

Left y-axis maximum

Type the maximum value of the left y-axis.

Show left grid lines

Select to show grid lines on the left y-axis.

Auto scale right y-axis

Select to activate auto scale. The scale of the right y-axis adapts itself to the displayed series.

Right y-axis minimum

Type the minimum value of the right y-axis.

Right y-axis maximum

Type the maximum value of the right y-axis.

Show right grid lines

Select to show grid lines on the right y-axis.

  • Trend Charts
  • Trend Chart Axes
  • Time Zone Modes in a Trend Chart
  • Trend Chart Settings Dialog Box – Series Tab
  • Trend Chart Settings Dialog Box – Calculation Tab
  • Trend Chart Y-Axis has Scale Problems
  • Trend Chart Live Update does not Work