earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendências
Versão do produto: 3.2, 3.3, 2022
22-07-2021

Trend Chart Settings Dialog Box – Calculation Tab

Use the Calculation tab to attach a calculation method to a series.

 
action_zoom_plus_stroke Calculations tab
Imagem: Calculations tab

Tabela: Calculations Tab

Component

Description

Data series

Displays all series in the trend chart. Select a series to display its presentation properties.

Calculation method

Select calculation method to calculate the recorded values before displaying the series in the trend chart.

Delta over period

Select to apply a period to the delta calculation method.

Period

Select the time span for which the calculation method is to be executed.

Custom period

When Custom period is selected, enter a custom time span for which the calculation method is to be executed.

Custom period alignment

When Custom period is selected, enter the time when you want the custom period to start.

  • Trend Charts
  • Calculation Methods
  • Trend Chart Settings Dialog Box – Axes Tab
  • Trend Chart Settings Dialog Box – Series Tab
  • Interrupted Series in the Trend Chart
  • Missing Trend Log Records