earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Trends
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
7/22/2021

Trend Chart Settings Dialog Box – X Axis Tab

Use the Axis tab in WebStation to change the x-axis settings of a trend chart.

 
action_zoom_plus_stroke X-axis tab
Figure: X-axis tab

Table: X-Axis Tab

Component

Description

Time mode

Select the time mode of the x-axis.

Start time

Enter the absolute start time when Time mode is configured to Absolute . This time is the leftmost point of the x-axis. For more information, see Configuring the X-axis with an Absolute Time Span .

Time span

Type the relative time span of the x-axis when Time mode is set to Relative . The rightmost point of the x axis is the current time. For more information, see Configuring the X-axis with a Relative Time Span .

Show gridlines for X-axis

Select True to show gridlines originating from the x axis scale. For more information, see Showing Trend Chart Grid Lines .

  • Trend Chart Axes in WebStation
  • Trend Series
  • Configuring the X-axis with an Absolute Time Span
  • Configuring the X-axis with a Relative Time Span
  • Showing Trend Chart Grid Lines
  • Automatically Configuring the Y-axis Scale
  • Manually Configuring the Y-Axis Scale
  • Trend Chart Settings Dialog Box – Series Tab
  • Trend Chart Settings Dialog Box – Left Axis Tab