You configure the time span of a trend chart X-axis to display the records that are recorded within a specific period of time.
In WebStation, in the System Tree pane, select the trend chart you want to configure.
On the Trend Chart toolbar, click the Settings button
In the Settings dialog box, click the X axis tab.
In the Time mode box, select Absolute (start and end time) .
In the Start time box, type the X-axis leftmost date and time.
Click OK .
Click Save .
The X-axis is now configured with an absolute time span.