earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface utilisateur

Interface utilisateur


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Tendances
Version produit : 2.0, 2.1, 3.0, 3.1
20/12/2018

Trend Chart Settings Dialog Box – Series Tab

Use the Series tab to configure the properties of the series in the trend chart.

 
action_zoom_plus_stroke Trend chart settings - series tab
Figure : Trend chart settings - series tab

Table : Series Tab

Component

Description

Display variable/trend log

Displays the referenced variable or trend log. To change the reference, browse to a different variable or trend log.

Data series

Displays all series in the trend chart. Select a series to display its presentation properties.

Series presentation

Select the presentation type of the series.

Assigned to y-axis

Select Left to attach the series to the left y-axis.

Weight

Type the weight of the line. The value has no correlation to any unit of measure.

Show markers

Select to display a marker for each record. Markers can only be shown for lines and discrete lines, not for digital and bars.

Show events

Select to present the series with event symbols.

Color

Enter the color of the series.

  • Courbes de tendance
  • Trend Chart Settings Dialog Box – Axes Tab
  • Trend Chart Settings Dialog Box – Calculation Tab