earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Trends
Product version: 2022, 2023, 2024
12/17/2021

Trend Chart Settings Dialog Box – Left Axis Tab

Use the Left axis tab in WebStation to change the settings for the left axis of a trend chart.

 
action_zoom_plus_stroke Left axis tab
Figure: Left axis tab

Table: Left Axis Tab

Component

Description

Show gridlines for left Y-axis

Select True to show grid lines originating from the left y-axis scale.  For more information, see Showing Trend Chart Grid Lines .

Left scale

Select if you want to display the axis linear or logarithmic.

Auto scale left Y-axis 

Select True to activate auto scale. The scale of the left Y-axis automatically adapts to the displayed series. For more information, see Automatically Configuring the Y-axis Scale .

Clear to deactivate auto scale. Manually scale the left axis by typing values in the Left Y-axis minimum and Left Y-axis maximum boxes.

Left Y-axis minimum 

Type the minimum value of the left y-axis. For more information, see Manually Configuring the Y-Axis Scale .

Left Y-axis maximum

Type the maximum value of the left y-axis. For more information, see Manually Configuring the Y-Axis Scale .

  • Trend Chart Series in WebStation
  • Trend Series
  • Trend Chart Series Menu
  • Trend Chart Settings Dialog Box – X Axis Tab
  • Trend Chart Settings Dialog Box – Series Tab