Use the Left axis tab in WebStation to change the settings for the left axis of a trend chart.
Component |
Description |
Show gridlines for left Y-axis |
Select True to show grid lines originating from the left y-axis scale. For more information, see Showing Trend Chart Grid Lines . |
Auto scale left Y-axis |
Select True to activate auto scale. The scale of the left Y-axis automatically adapts to the displayed series. For more information, see Automatically Configuring the Y-axis Scale . Clear to deactivate auto scale. Manually scale the left axis by typing values in the Left Y-axis minimum and Left Y-axis maximum boxes. |
Left Y-axis minimum |
Type the minimum value of the left y-axis. For more information, see Manually Configuring the Y-Axis Scale . |
Left Y-axis maximum |
Type the maximum value of the left y-axis. For more information, see Manually Configuring the Y-Axis Scale . |