The Trend Log Comparison report provides a way for you to compare the output of the trend logs associated with a data point, such as the kilowatts for a power meter. The report provides similar reporting as the Trend Chart, however, you can export the report, schedule the report, and run the report using a Web browser and without access to WorkStation.
The following table shows the input parameters for the report.
Input Parameters |
Description |
Start report date/time |
Specifies the start date and time for tracking all trend log data points. |
End report date/time |
Specifies the end date and time for tracking all trend log data points. |
Date filter |
Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent. For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days. Select Fixed date if you entered a Start report date/time and an End report date/time . |
Ext. trend logs |
Specifies the extended trend logs that you want to compare. |
Report view |
Specifies the format, such as a table, for displaying the report. |