earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 2023
12/17/2022

User Account Group – Software Permissions Tab

Use the Software Permissions tab to add software permissions to a user account group by adding paths and assigning command permissions to the group.

 
action_zoom_plus_stroke Software permissions tab
Figure: Software permissions tab

Table: Software Permissions Tab

Component

Description

 
action_zoom_plus_stroke

Add

Click to add a path to the list of paths the user account group can access.

 
action_zoom_plus_stroke

Add System

Click to add the the system's top level path.

Path

Displays the paths that have been defined for the user account group.

Permission

Click to assign a permission level to a path you have selected. For more information, see Software Permissions Rules Management .

Properties

The access to the Property Permissions dialog box where you define the level of permissions to object properties for the user account group.

 
action_zoom_plus_stroke

Click to access the Property Permissions dialog box. For more information, see Property Permissions .

Relative path permissions

Browse to a folder structure to grant a specific set of permissions to a user account group to all the folders accessible in a predefined path and its folder structure.

Owner

Displays the user account group the path has been added to. Owner can be one or more user account groups the user account is a member of or the user account.

 
action_zoom_plus_stroke

Delete

Click to remove a path from the list of paths the user account group can access. For more information, see Confirm Delete Dialog Box .

 
action_zoom_plus_stroke

Add

Click to add a path to the type permission object the user account group can access

 
action_zoom_plus_stroke

Delete

Click to remove a type permission from the list of paths the user account group can access. For more information, see Confirm Delete Dialog Box .

Type permission

Displays the type permissions that have been defined for the user account group.

Category

Click a category to display the commands included in the category.

Command

Displays all commands for the category.

Decription

Displays the description of the command.

Permission

Select a permission level for the command.

Category

Displays categories included in the category.

Command

Displays all commands of the categories included in the category

Permission

Displays a permission level for the command.

Owner

Displays the user account groups the commands have been added to.

  • Software Permissions, User Accounts, and User Account Groups
  • Software Permissions Rules Management
  • Property Permissions
  • Confirm Delete Dialog Box
  • Property Permissions Dialog Box