Building Operation is equipped with three types of utilities: Signal Generators, Simple Math Operators, and Timed Force objects. These utilities are used for testing, for example, trend logs and alarms.
For more information, see WorkStation .
Signal Generator is used to create a sinusoidal, square, or saw tooth curve. Signal generator can also be used to generate a setpoint, an alarm, or an event.
Simple Math Operator is used to add, subtract, multiply, and divide a one value from another.
Timed Force objects are utility objects that force an override of the actual value of an analog, digital, or multistate output for a period of time specified either as a time duration or as a selected end date and time.
For more information, see Timed Force Objects .