earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WorkStation, WebReports
Funktionaliteter: Rapporter
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021-12-16

Viewing a Default Report with Multiple Objects

You view a default report with multiple objects to see a report about more than one object of the same type, for example, two or more user accounts.

Visa mer
action_close

A default report provides information about alarms, generic objects, EcoStruxure BMS servers, trend logs, and user accounts. The report is formatted according to a template that is assigned to an EcoStruxure Building Operation object type. You view default reports in WorkStation using the View...Report submenu. You cannot view default reports using a Web browser.

When you install WebReports, default report templates are assigned to the following EcoStruxure Building Operation object types:

  • Alarm

  • Generic Object

  • EcoStruxure BMS server

  • Trend log

  • User Account

To view a default report for a single object, you select the object and then the View...Report submenu in WorkStation. While in List View, you can select more than one object of the same type and generate a report for both objects. For example, suppose you want to see a default report about an Out of Range Alarm and an Inside Range Alarm. You can select both alarms in List View and then run View....Report. The default report generates output about both alarms in one report.

You assign templates to object types for the default reports using the Assign Default Reports menu option at the WebReports Web site.

To view a default report with multiple objects
  1. In WorkStation, in List View , select two or more objects of the same type, such as two user accounts.

  2. On the Actions menu, point to View and then click Report .

  • Default Reports
  • Assigning a Default Report Template
  • Assign Default Reports Page
  • Viewing a Default Report in WorkStation