Funzionalità: Funzionalità di base
Versione del prodotto: 3.2, 3.3, 2022
15/10/2020

Viewing Shortcut Properties

You view the properties of a shortcut in order to confirm or change the target of the shortcut.

Mostra di più
action_close

When you have created a shortcut in a folder or on an EcoStruxure BMS server using the File-New-Shortcut submenu or the context menu New-Shortcut option, you must then also assign a target to the shortcut. It is not necessary to assign a target to a shortcut after using any other shortcut creation method.

When you delete a target object, the forward reference in all shortcuts referencing that target object is removed. Also, the shortcut object icon changes to display the shortcut overlay icon only (a small arrow in a square).

When you delete a shortcut object, the (backwards) reference held in the target object is removed.

When you move a target object, the shortcuts referencing that target are updated with the new target path in their (forward) target object reference. When you move a shortcut object, the (backwards) reference held in the target object is updated with the new path.

When you rename a target object, the shortcuts referencing that target are updated with the new target path. If you rename a shortcut object, the (backwards) reference held in the target object is updated with the new path.

When you duplicate a shortcut object, the (backwards) reference held in the common target object is updated with the additional path to the new shortcut. Per maggior informazioni, consulta Configuring the Target of a Shortcut .

To view the properties of a shortcut
  • In the System Tree pane, right-click the shortcut and then click Shortcut Properties .

Avviso
  • You cannot view the properties of a shortcut by selecting the Properties command. You must select the Shortcut Properties command.

  • General Information Properties – Basic Tab
  • References Tab
  • Shortcut Creation
  • Shortcut Properties – Basic Tab
  • Configuring the Target of a Shortcut