earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Conceito

Conceito


Produtos: WebReports
Funcionalidades: Relatórios
Versão do produto: 3.0, 3.1, 3.2, 3.3
16-12-2021

Windows Roles and Features

The WebReports installation requires you to select certain roles and services to install on the Application Server and the Web Server (IIS), and to install .NET Framework 3.5 and .NET Framework 4.x features. You install these roles and features using the Server Manager in Windows Server 2008, Windows Server 2012, Windows Server 2012 R2, or Windows Server 2016. For Windows 7, Windows 8.1, and Windows 10, you configure the roles and features using Control Panel. It is recommended that you install these roles and features before you install SQL Server.

Server Manager is accessible from the Start screen or from the desktop (task bar). You begin by adding the .NET Framework 3.5 features, the IIS server role and selecting the role services, and then you add .NET Framework 4.x features. The following figures show the features that must be selected when configuring Roles and Features for Windows Server 2012, Windows Server 2012 R2, or Windows Server 2016. For Windows 7, Windows 8.1, or Windows 10, you configure the roles and features using Control Panel.

To install .NET Framework 3.5 on Windows 8.1 or Windows 10 and Windows Server 2012, Windows Server 2012 R2, or Windows Server 2016, enter the following source path:

dism /online /enable-feature /featurename:NetFX3 /all /Source:e:\sources\sxs /LimitAccess

Nota

In this example, the Windows Server 2012 setup CD is in the e drive. Use the appropriate drive in the path for your PC configuration.

 
action_zoom_plus_stroke .Net Framework 3.5 installation (Windows Server 2012)
Imagem: .Net Framework 3.5 installation (Windows Server 2012)
 
action_zoom_plus_stroke Web Server (IIS) server role selection (Windows Server 2012)
Imagem: Web Server (IIS) server role selection (Windows Server 2012)
 
action_zoom_plus_stroke Features Selection (Windows Server 2012)
Imagem: Features Selection (Windows Server 2012)
 
action_zoom_plus_stroke Application Server role services selection (Windows Server 2012)
Imagem: Application Server role services selection (Windows Server 2012)
 
action_zoom_plus_stroke Windows Roles and Features successful installation page (Windows Server 2012)
Imagem: Windows Roles and Features successful installation page (Windows Server 2012)

For Windows Server 2008, you begin by adding the IIS server role and selecting the role services, and then you add the .NET Framework 3.5.1 features. The following figures show the settings that must be selected when configuring windows roles and features.

 
action_zoom_plus_stroke Web Server (IIS) server role selection
Imagem: Web Server (IIS) server role selection
 
action_zoom_plus_stroke  .NET Framework configuration
Imagem: .NET Framework configuration
 
action_zoom_plus_stroke Window roles and features - successful installation page
Imagem: Window roles and features - successful installation page

For Windows 7, Windows 8.1, and Windows 10, you can configure the roles and features using Control Panel. In Control Panel, navigate to Programs , and select Turn Windows features on or off . Select .NET Framework 3.5 (includes .NET 2.0 and 3.0) , .NET Framework 4.7 Advanced Services , and Internet Information Services .

 
action_zoom_plus_stroke Configuration of roles and features for Windows 10
Imagem: Configuration of roles and features for Windows 10
  • WebReports Overview
  • WebReports Installation Overview
  • Features Dialog Box for Windows Server 2012
  • Features Dialog Box for Windows Server 2008
  • Role Services Dialog Box
  • SQL Server Installation Settings