earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: WebReports
Funcionalidades: Relatórios
Versão do produto: 3.0, 3.1, 3.2, 3.3
16-12-2021

Features Dialog Box for Windows Server 2012

Use the Features dialog box to select the .NET Framework 3.5 and .NET Framework 4.x features for installation. The features are required for the WebReports installation, and it is recommended that you install the services before you install SQL Server.

 
action_zoom_plus_stroke

Tabela: Features Dialog Box

Component

Description

.NET Framework 3.5 Features

Select to install all .NET Framework 3.5 Features.

.NET Framework 3.5

Select to install .NET Framework 3.5.

.NET Framework 4.x Features

Select to install all .NET Framework 4.x Features.

.NET Framework 4.x

Select to install .NET Framework 4.x.

  • Windows Roles and Features